While debugging there is an issue called "An error has occurred. See error log for more details."

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

While debugging there is an issue called "An error has occurred. See error log for more details."

1,385 次查看
pankajprasad100
Contributor III

Hello, 

 

Previously I posted my query in below link

 

While debugging there is an issue called "An error... - NXP Community

 

After reinstall also facing same issue

 

I am working on urgent project quick response would be highly appreciated.

0 项奖励
回复
1 回复

1,377 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi pankajprasad100,

In the Debug Configurations dialog box, select the required debug configuration. The name of the debug configuration is composed of the project name, debugging interface and build configuration. The configuration settings appear on the tabs:

If I select hello_world_s32k144_debug_ram_pemico, the Name will shown in right side.

Main.png

But don't know why the Name is blank at your side.

pankajprasad100_2-1611031108145.png
These configurations are set by default after selected.

Debugger.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复