While debugging there is an issue called "An error has occurred. See error log for more details."

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

While debugging there is an issue called "An error has occurred. See error log for more details."

1,347 Views
pankajprasad100
Contributor III

Hello, 

 

Previously I posted my query in below link

 

While debugging there is an issue called "An error... - NXP Community

 

After reinstall also facing same issue

 

I am working on urgent project quick response would be highly appreciated.

0 Kudos
Reply
1 Reply

1,339 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi pankajprasad100,

In the Debug Configurations dialog box, select the required debug configuration. The name of the debug configuration is composed of the project name, debugging interface and build configuration. The configuration settings appear on the tabs:

If I select hello_world_s32k144_debug_ram_pemico, the Name will shown in right side.

Main.png

But don't know why the Name is blank at your side.

pankajprasad100_2-1611031108145.png
These configurations are set by default after selected.

Debugger.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply