What is the mpc 5777c microcontroller flash programming tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the mpc 5777c microcontroller flash programming tool

3,323 Views
192064963
Contributor II

hi, What is the mpc 5777c microcontroller flash programming tool?   I did not find a flash programming tool for the MPC5777c processor.  thsanks

 

 

 

 

 

 

 

0 Kudos
Reply
6 Replies

3,290 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Along with recommendations from our website below you could also take a look on third party providers’ website:

https://www.segger.com

http://www.lauterbach.com

http://www.pemicro.com

https://www.pls-mc.com

 

Also I could point out to some other solution of production programming (direct programming of MCU over ZIF socket):

https://www.elnec.com

 

Regarding S32DS 2.1 - it natively supports P&E Multilink/Cyclone/OpenSDA. 

Lauterbach, iSystem, and PLS can be supported by plugin:
https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32-Design-Studio-for-Power-Architectu...

 

0 Kudos
Reply

3,316 Views
192064963
Contributor II
Does the S32 Flash Tool 2.3.3 tool is support MPC5777C microcontrollers.
0 Kudos
Reply

3,293 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

No, following devices are supported.

2.3 Supported devices
Flash Tool provides support for the following NXP devices:
• S32R41
• S32R45
• S32G2xx
• S32G3xx
• SAF85xx
• SAF86xx
• S32R47
• S32N5
• S32Z2/E2

0 Kudos
Reply

3,042 Views
192064963
Contributor II
Solved. Thank you very much.
0 Kudos
Reply

3,275 Views
192064963
Contributor II
Thank you for your reply. We now need to provide the customer with a .bin file burning program. We don't want to give them the source code. However, S32DS 2.1 requires a code project to compile and download. Are there any other ways to directly download the .bin file?
0 Kudos
Reply

3,232 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-download-separate-elf-srec-hex-f...

Usually we use .elf or .srec for these purposes. .bin is is not usually used with modern MCUs.

0 Kudos
Reply