Using semihosting with custom printf

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using semihosting with custom printf

ソリューションへジャンプ
4,950件の閲覧回数
Joao_Roscoe
Contributor III

Hello, there,

I'm working in a project that will use all therr UARTS in S32K144, and one of them will be used as a simple console, with custom print code - not libc printf.

At this point, I'm still using S32K144EVB, and I would like to use semihosting console - so I looked at the EVB schematics, and saw that PTC6 and PTC7 are connected to UART1_TX_TGTMCU_R and UART1_RX_TGTMCU_R nets, and to MK20DX128VFM5, which implements OpenSDA.

I patched my custom print code (which works with a regular UART adapter connected to EVB pins) to use UART1, and configured PTC6 and PTC7 as follows:
/* Tx pin configuration data */
.tx_pin_cfg.base = PORTC,
.tx_pin_cfg.pinPortIdx = 7U,
.tx_pin_cfg.pullConfig = PORT_INTERNAL_PULL_NOT_ENABLED,
.tx_pin_cfg.driveSelect = PORT_LOW_DRIVE_STRENGTH,
.tx_pin_cfg.passiveFilter = false,
.tx_pin_cfg.mux = PORT_MUX_ALT2,
.tx_pin_cfg.pinLock = false,
.tx_pin_cfg.intConfig = PORT_DMA_INT_DISABLED,
.tx_pin_cfg.clearIntFlag = false,
.tx_pin_cfg.gpioBase = NULL,
.tx_pin_cfg.digitalFilter = false,
/* Rx pin configuration data */
.rx_pin_cfg.base = PORTC,
.rx_pin_cfg.pinPortIdx = 6U,
.rx_pin_cfg.pullConfig = PORT_INTERNAL_PULL_NOT_ENABLED,
.rx_pin_cfg.driveSelect = PORT_LOW_DRIVE_STRENGTH,
.rx_pin_cfg.passiveFilter = false,
.rx_pin_cfg.mux = PORT_MUX_ALT2,
.rx_pin_cfg.pinLock = false,
.rx_pin_cfg.intConfig = PORT_DMA_INT_DISABLED,
.rx_pin_cfg.clearIntFlag = false,
.rx_pin_cfg.gpioBase = NULL,
.rx_pin_cfg.digitalFilter = false,

}

I alse have semihost enabled in project properties, and I'm using no IO newlib_nano, since I'm using a custom print code - not libc printf.

While debugging, however, I'm not getting anything in semihost console.

What am I missing here? What UART parameters (BAUD, nbits, parity, flow control) shouln I use?

Best regards,

Joao

0 件の賞賛
返信
1 解決策
4,931件の閲覧回数
Joao_Roscoe
Contributor III

Well, it turns out I was mixing up two completely different concepts: S32K144EVB does allow routing UART1 through OpenSDA - but that's not semihosting. When using semihosting, a real serial port of the MCU under debugging is not involved, and libc will talk directly to OpenSDA.

In fact, I've just 'found' a virtual COM in my debug PC, hooked a terminal emulator to it and bingo, it's working.

I imagine that this post could possible be useful for someone in teh future.

Thank you,

Joao

 

元の投稿で解決策を見る

3 返答(返信)
4,942件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi,

The Semihosting console requires STD C library with I/O support - the output data aren't related to any UART port - it is GDB server/client feature. 

 

Jiri  

 

 

4,940件の閲覧回数
Joao_Roscoe
Contributor III

Nice. I'll give it a try ASAP.

And what about the serial parameters?

Thank you for your time,

Joao

0 件の賞賛
返信
4,932件の閲覧回数
Joao_Roscoe
Contributor III

Well, it turns out I was mixing up two completely different concepts: S32K144EVB does allow routing UART1 through OpenSDA - but that's not semihosting. When using semihosting, a real serial port of the MCU under debugging is not involved, and libc will talk directly to OpenSDA.

In fact, I've just 'found' a virtual COM in my debug PC, hooked a terminal emulator to it and bingo, it's working.

I imagine that this post could possible be useful for someone in teh future.

Thank you,

Joao