Using S32DS with jLink debugger - how to attach to a running device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using S32DS with jLink debugger - how to attach to a running device

2,886件の閲覧回数
freddy_ben-zeev
Contributor IV

I'd like to attach the jLink debugger to my running device (an S32K148) on our board without resetting the device. I've checked the "Connect to running target" checkbox on the Debug Configuration window Debugger tab, and tried to uncheck various checkboxes on the Startup tab but the device is always reset when I press Debug. On the EVB board with the pemicro debugger there is an "Attach to running target" on the Debugger tab which works just fine, but I need to use the jLink on our board. Any idea how to set this up?

Freddy

1 返信

2,729件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi Freddy, 

this is known issue - but I'm afraid, that not solved yet - https://community.nxp.com/message/1155473  

Jiri