Unable to debug s32k146 EVM getting opensda error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to debug s32k146 EVM getting opensda error

Jump to solution
1,669 Views
Sukumar21
Contributor III

I have got my new S32k146 EVM. and also downloaded s32 design studio 3.4. I am just trying to load lpspi(lpspi_dma_s32k146) program in evm board. I have also updated OPENSDA as per in link below:

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Update-OpenSDA-Firmware-on-EVB/t...

But still i cannot debug a program from S32 design studio:

following error is displayed

Sukumar21_0-1696064107237.pngSukumar21_0-1696064107237.png

 

 

Labels (1)
0 Kudos
Reply
1 Solution
1,636 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please refer to the discussion in S32K144 D2 RED LED is ON always


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,637 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please refer to the discussion in S32K144 D2 RED LED is ON always


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply