Unable to debug s32k146 EVM getting opensda error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to debug s32k146 EVM getting opensda error

ソリューションへジャンプ
1,699件の閲覧回数
Sukumar21
Contributor III

I have got my new S32k146 EVM. and also downloaded s32 design studio 3.4. I am just trying to load lpspi(lpspi_dma_s32k146) program in evm board. I have also updated OPENSDA as per in link below:

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Update-OpenSDA-Firmware-on-EVB/t...

But still i cannot debug a program from S32 design studio:

following error is displayed

Sukumar21_0-1696064107237.png

 

 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,666件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please refer to the discussion in S32K144 D2 RED LED is ON always


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,667件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please refer to the discussion in S32K144 D2 RED LED is ON always


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信