UART error during debugging time

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

UART error during debugging time

3,287 次查看
MohitManvar
Contributor III

Hello,

I am using S32K142 Eval board for testing of mcal.

I tried with example project of ADC  (adc_swtrigger_s32k142).

during debugging when I starting communication it is giving me following error.

 

MohitManvar_0-1688649502609.png

 

plz provide solution for removing error, so I can see Adc value on console/terminal window.

 

Thanks!

0 项奖励
回复
3 回复数

3,239 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @MohitManvar .

Sorry for late reply. 

Please can you provide me more information. 

And also please can you provide the workspace log from the path

C:\Users\Public\[workspace]\.metadata  (or wherever your relevant workspace is located). 

Plus, Please can you share the installation details as well from : Help -> S32Ds Extension and Updates -> Installation details. 



Mehul_Patel_NXP_0-1689022206085.png

Thank you. Kind regards. 

- Mehul Patel

 

 

3,207 次查看
MohitManvar
Contributor III

Hello Mehul,

as I mentioned earlier, I am using S32DS with S32K142 microcontroller. I was trying to run examples code for ADC which is already available in S32DS. As per code, from Potentiometer(ADC) voltage is being read and displayed on screen. for Display purpose UART configuration is used in code. but after successfully build and on debug window mentioned screenshot is shown.

 

as per your reply I'm also attaching log file and installation detail.

 

Thanks!

0 项奖励
回复

2,975 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

if the issue is still actual - which terminal are you using for UART messages? 

0 项奖励
回复