S32DS 2.2中ProcessorExpert被disable

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32DS 2.2中ProcessorExpert被disable

4,604 次查看
Zhuang
Contributor I

工程中的ProcessorExpert被disable了,打开引脚、时钟、外设的配置都是灰色的。

点击生成代码时会报错如附件。

请问这种情况可能是什么问题导致的?该如何解决?

0 项奖励
回复
3 回复数

4,593 次查看
Zhuang
Contributor I

The ProcessorExpert in the project is disabled, and the configuration of opening pins, clocks, and peripherals are all gray.

Click Generate code, error as attached.

What might be the cause of this situation? How to fix it?

This is not the case with routines that create new RTD driver.

0 项奖励
回复

4,383 次查看
jiri_kral
NXP Employee
NXP Employee

Hi,

please check the processor expert settings in Project Properties: 

jiri_kral_0-1696321857482.png

 

It is possible, that your project is based on older SDK which is not installed. 

 

0 项奖励
回复

4,601 次查看
Zhuang
Contributor I

建立新的RTD的例程是不会有这种情况的。

0 项奖励
回复