The S32FlashTool in ubuntu does not support S32G274A to write EMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The S32FlashTool in ubuntu does not support S32G274A to write EMMC

Jump to solution
1,893 Views
B0
Contributor I

After installing S32DS 3.4 on Ubuntu 18.4, but I found that S32G274A is not supported by S32FlashTool, I only found the following files from S32FlashTool/target  

S32S247TV.bin S32V234.bin

Can you provide an S32FlashTool that supports S32G274A to write EMCC? 

0 Kudos
Reply
1 Solution
1,818 Views
B0
Contributor I

Hello Mike,

    After I  install the S32Gxx Development Package, I can use it now.

Thanks

Xiaobo

View solution in original post

0 Kudos
Reply
2 Replies
1,819 Views
B0
Contributor I

Hello Mike,

    After I  install the S32Gxx Development Package, I can use it now.

Thanks

Xiaobo

0 Kudos
Reply
1,843 Views
mikedoidge
NXP Employee
NXP Employee

Hello Xiaobo,

Please ensure you have installed the S32Gxx Development Package into S32 Design Studio. The S32G support files for S32 Flash Tool are delivered with this package.

Best Regards,

Mike

0 Kudos
Reply