The S32FlashTool in ubuntu does not support S32G274A to write EMMC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

The S32FlashTool in ubuntu does not support S32G274A to write EMMC

跳至解决方案
1,933 次查看
B0
Contributor I

After installing S32DS 3.4 on Ubuntu 18.4, but I found that S32G274A is not supported by S32FlashTool, I only found the following files from S32FlashTool/target  

S32S247TV.bin S32V234.bin

Can you provide an S32FlashTool that supports S32G274A to write EMCC? 

0 项奖励
回复
1 解答
1,858 次查看
B0
Contributor I

Hello Mike,

    After I  install the S32Gxx Development Package, I can use it now.

Thanks

Xiaobo

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,859 次查看
B0
Contributor I

Hello Mike,

    After I  install the S32Gxx Development Package, I can use it now.

Thanks

Xiaobo

0 项奖励
回复
1,883 次查看
mikedoidge
NXP Employee
NXP Employee

Hello Xiaobo,

Please ensure you have installed the S32Gxx Development Package into S32 Design Studio. The S32G support files for S32 Flash Tool are delivered with this package.

Best Regards,

Mike

0 项奖励
回复