TRK KEA64 with external clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TRK KEA64 with external clock

1,033件の閲覧回数
hanisamara
Contributor III

Hello, 

i want to use the external clock on the TRK KEA64 board (FEE mode), but the software hangs on this loop:

while(!(OSC_CR & OSC_CR_OSCINIT_MASK));

i have the revision B and D Boards and i get the same result on both!

the oscillator is built on both boards but it seems like there is no clock? 

i am using S32 DS and the file ics.c from the SDK.

i there any thing i miss to set/enable? 

thanks in advance, 

Hani

ラベル(1)
タグ(3)
0 件の賞賛
返信
0 返答(返信)