Shared memory in multi-core projects

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Shared memory in multi-core projects

4,695件の閲覧回数
helferog
Contributor II

Hello 

I am currently developing a multicore system with the S32R274 in S32 Studio.

As I have seen, in S32Studio for each core a separate project is created. For me this means, it is not possible to build up code for the second core, which knows addresses or variables, also known by the first core. Is that wright?

Or Is there a way to avoid redefining global variables in code and instead work with 1 real global definition?

Is there a way to dynamically link the addresses of linker script files from different cores(projects)?

What way would you suppose to handle the shared memory?

Thanks and best regards

Roger

0 件の賞賛
返信
2 返答(返信)

3,832件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hello Roger, 

He is another shared memory example using slightly different method. This example is for S32DS Power v1.2. 

https://community.nxp.com/docs/DOC-335344 

Jiri

0 件の賞賛
返信

3,832件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

please check the example below. It shows, how to modify linker file and also, how to access the variable in shared memory using different cores.

https://community.nxp.com/docs/DOC-329941 

If you have any other questions, please feel free to write me back.

Regards,

Martin

0 件の賞賛
返信