SDK missing though RTD installed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK missing though RTD installed

1,428 Views
hns80
Senior Contributor I

I am using S32DS 3.5 and installed RTD S32K358 3.0.0 3.0.0.202212220514 through the updatesite zip file and it is displayed when I show installation details.

When I import a project developed with it, I receive an error that the SDK path for RTD is not found:

SDK PlatformSDK_S32K3_3_0_0_S32K358_M7_0_0_3.0.0_PATH is not found in workspace

How can I make S32DS aware that the RTD is available?

I had a similar issue under 3.4 with another version of the RTD. The only way I was able to resolve it that time was to completely uninstall and re-install everything. Hopefully there is a better method?

 

 

 

0 Kudos
Reply
1 Reply

1,299 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @hns80 , 

 

Please can you share more details to understand the issue. 

 

Please can you provide the log of S32DS workspace from

  C:\Users\Public\[workspace_name]\.metadata ( Or wherever your workspace is located) 

Thank you. Best regards. 

 

- Mehul Patel. 

0 Kudos
Reply