SDK cannot be found when creating a new Application project on S32DS3.5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK cannot be found when creating a new Application project on S32DS3.5

Jump to solution
2,668 Views
ukn
Contributor I

I recently installed S32DS3.5 and the attached image contains the  all the packages I installed along with S32DS. When I try to create an application project, I cannot see any SDK in it. Also, when I try to create a new project from example, I cannot see any examples. How do I get the SDK? should I install anything else?

 

ukn_0-1695309485219.pngukn_0-1695309485219.png

 

0 Kudos
Reply
1 Solution
2,594 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @ukn 

I ask you to please provide an image of the information provided in the installation details. This situation usually happens when it is not installed all the necessary packages or if you do not have the right version of these. 

 

B.R.

VaneB

View solution in original post

0 Kudos
Reply
3 Replies
2,174 Views
terry-1987
Contributor I

how you fix the issue?

0 Kudos
Reply
2,595 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @ukn 

I ask you to please provide an image of the information provided in the installation details. This situation usually happens when it is not installed all the necessary packages or if you do not have the right version of these. 

 

B.R.

VaneB

0 Kudos
Reply
2,589 Views
ukn
Contributor I

Hi @VaneB ,

 

I reinstalled the S32DS3.5 and the related packages and it fixed the issue. 

Thanks

0 Kudos
Reply