SDK cannot be found when creating a new Application project on S32DS3.5

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SDK cannot be found when creating a new Application project on S32DS3.5

跳至解决方案
2,699 次查看
ukn
Contributor I

I recently installed S32DS3.5 and the attached image contains the  all the packages I installed along with S32DS. When I try to create an application project, I cannot see any SDK in it. Also, when I try to create a new project from example, I cannot see any examples. How do I get the SDK? should I install anything else?

 

ukn_0-1695309485219.png

 

0 项奖励
回复
1 解答
2,625 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @ukn 

I ask you to please provide an image of the information provided in the installation details. This situation usually happens when it is not installed all the necessary packages or if you do not have the right version of these. 

 

B.R.

VaneB

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,205 次查看
terry-1987
Contributor I

how you fix the issue?

0 项奖励
回复
2,626 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @ukn 

I ask you to please provide an image of the information provided in the installation details. This situation usually happens when it is not installed all the necessary packages or if you do not have the right version of these. 

 

B.R.

VaneB

0 项奖励
回复
2,620 次查看
ukn
Contributor I

Hi @VaneB ,

 

I reinstalled the S32DS3.5 and the related packages and it fixed the issue. 

Thanks

0 项奖励
回复