SBC Board: Trouble executing grabber PreStart()

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SBC Board: Trouble executing grabber PreStart()

2,010 次查看
RobShand
Contributor II

I'm a newbie to S32DS.

 

THE ENVIRONMENT

I have S32DS 3.4.3 with VSDK 1.7 installed, and I have the SBS-S32V234 development board, which has two MIPI camera's connected. The camera type is OV10640CSP-S32V

 

THE CHALLENGE

As a first step, I want to stream video from one of the camera's to the HDMI output

 

THE SETUP

I first created an ISP project based upon ov10640_default, and emitted it to my Linux A53 application project without problems.

Following guidance from an NXP tutorial, I have tailored some defines in isp_user_define.h for the camera as follows, which I think is correct:

#define WIDTH_DDR 1288
#define HEIGHT_DDR 732
#define M_NUM_OUT_LINES (732)
#define MULTITRIGGER 0
#define DDR_OUT_BUFFER_CNT 6
#define LOOP_NUM 30

#define DCU_BPP DCU_BPP_24

In addition, this is what my io_config() function looks like:

void io_config(sdi_grabber *lpGrabber)
{
   // *** prepare IOs ***
   sdi_FdmaIO *lpFdma = (sdi_FdmaIO*)lpGrabber->IoGet(SEQ_OTHRIX_FDMA);
   // modify DDR frame geometry to fit display output
   SDI_ImageDescriptor lFrmDesc = SDI_ImageDescriptor(WIDTH_DDR, HEIGHT_DDR, RGB888);
   lpFdma->DdrBufferDescSet(FDMA_IX_CAM_OUTPUT, lFrmDesc);
   //*** allocate DDR buffers ***
   lpFdma->DdrBuffersAlloc(FDMA_IX_CAM_OUTPUT, DDR_OUT_BUFFER_CNT);
}

THE PROBLEM

After compiling the app, and entering debug mode, stepping through io_config is fine, but the subsequent call returns -1, which indicates an error:

LIB_RESULT result = lpGrabber->PreStart();

 

I'm a bit unsure of what else I can look for to diagnose this, and the error code is quite unhelpful.

Can anybody think of a few things I can try or check to resolve this?

Kind Regards,

Rob

标记 (1)
0 项奖励
回复
2 回复数

1,916 次查看
Yu_Fu
NXP Employee
NXP Employee

Hi, Rob,

     What did you change in your project except "isp_user_define.h"?  Pls be careful when you modify ISP, because some change may be not supported by camera.

Yu

0 项奖励
回复

1,912 次查看
RobShand
Contributor II

Hi Yu,

Thanks for responding. I actually resolved the problem. The ISP does not generate the proper source for this camera, so I wrote my own one, which I submitted to NXP who are keen to build it in their nest BSP release.

Kind Regards,

Rob

0 项奖励
回复