S32R274 debugging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32R274 debugging

Jump to solution
4,397 Views
chidvilas_y
Contributor II

Hi,

I've installed the S32 Design Studio for Power Architecture, Version: 1.2, Build id: 170613. 

I've connected S32R274RRUEVB(daughter board only) to PC using USB mini cable.

I am able to build the example projects in SDK but not able to debug those.

How to load the elf files on the board and run/debug them?

Should I have to use any external debuggers(PEmicro/Segger)?

Is there any internal debugger present on the board(OpenSDA)?

Thanks,

Chidvilas

0 Kudos
Reply
1 Solution
4,044 Views
jiri_kral
NXP Employee
NXP Employee
3 Replies
4,044 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

the Mini USB is converter to UART.  You need to use external probe like PE Micro. 

Jiri

0 Kudos
Reply
4,044 Views
chidvilas_y
Contributor II

Thanks for the info, Can you please suggest me the model of the probe, like PE Micro USB MULTILINK / USB MULTILINK FX?

Can you also provide me the differences between them?

Thanks,

Chidvilas

0 Kudos
Reply
4,044 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

in my opinion PE Micro USB Multilink is better choice for future use. 

Here are details: 

PE Micro USB Multilink:

PEmicro - P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Develop... 

PE Micro USB Multilink FX:

PEmicro - P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Develop... 

Jiri