S32K3 Design Studio v3.5 activation issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 Design Studio v3.5 activation issue

ソリューションへジャンプ
3,810件の閲覧回数
ec23930
Contributor I

Hello,

I have re-installed the S32K3 Design Studio 3.5 (using S32DS.3.5_b220726_win32.x86_64.exe) in my notebook and encountered activation issue as below. The installation could not complete after the message had popped up. My notebook is with Windows 11. Tried both online & offline activation.
It happened after I had un-installed the S32K3 Design Studio v3.5 and re-installed it in the same machine.
I would like to know if any way to fix it.

Thank you.

S32K3 DS activation error.png

0 件の賞賛
返信
1 解決策
3,784件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @ec23930 , 

 

I am not sure why, but as I see, you had only 1 license was already used, so you were no longer able to raise request for the activation. I have increase license quantity to 100, so 99 licenses are available now. 

 

Please can you check whether you are able to use the license or not. If any issue please let us know.

 

Thank you. Kind regards. 

 

- Mehul Patel 

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
2,793件の閲覧回数
aewt
Contributor I

Hi,

I have the same issue; I installed S32DS on a GNU/Linux VM and I need to install it again on a Win10 VM but I have only 1 license. If possible, could you please increase my licenses for S32DS?

Many thanks and kind regards,

Ali

0 件の賞賛
返信
3,463件の閲覧回数
sungyeon
Contributor I

I have same issues. How can I solve it?

 

0 件の賞賛
返信
3,785件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @ec23930 , 

 

I am not sure why, but as I see, you had only 1 license was already used, so you were no longer able to raise request for the activation. I have increase license quantity to 100, so 99 licenses are available now. 

 

Please can you check whether you are able to use the license or not. If any issue please let us know.

 

Thank you. Kind regards. 

 

- Mehul Patel 

0 件の賞賛
返信
2,810件の閲覧回数
adalberto1
Contributor II

Hello,

I have S32DS installed on Windows, and would also like to install it on Linux.  Is there a way to increase my license quantity to be able to do that?

I've tried, and get an error explaining I have exceeded the quantity of my licenses.

0 件の賞賛
返信
3,555件の閲覧回数
anakha
Contributor III
How can I change license quantity?
0 件の賞賛
返信
3,749件の閲覧回数
ec23930
Contributor I
Hi Mehul,

The installation process can now be completed and the problem has been fixed.
Thank you!
0 件の賞賛
返信