S32K146 EVB - P&E Connection Assistant

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K146 EVB - P&E Connection Assistant

2,117 次查看
HancenChen
Contributor II

Dear Officer,

We had a SK32K146 EVB board working fine previous, and the demo can be run.

After I downlown my program(via OpenSDA-USB port) in S32DS, at the first, I can debug it. But some error in my program, the breakpoint jump to the default_isr. so I disconnect it and modify my source code. Then I download again. However, the below dialog box will be shown. 

HancenChen_0-1630639481664.pngHancenChen_0-1630639481664.png

I close it, the new dialog box as below:

HancenChen_0-1630643744863.pngHancenChen_0-1630643744863.png

 

the debugger configuration as below:

HancenChen_1-1630641025368.pngHancenChen_1-1630641025368.png

 

 

I have search the related topic on NXP Community, may be they are no help. So I post it again.

The 5V power is OK(J107).

MCU 5V (J15) is OK.

I debug the MCAL, the main function is :

HancenChen_2-1630640294091.pngHancenChen_2-1630640294091.png

It may be the PLL clock is not init normally.

Please give me some help, I'm at a loss, because the EVB was reveived last day, and it can not use.

Thanks a lot !

 

0 项奖励
回复
1 回复

2,101 次查看
HancenChen
Contributor II

I have already solved this problem.

At first, I download a J-Link Commander, and want to erase the chip. But can't connect to target. And the command line shows that "Communication error while accessing MDM-AP."

So I search it in community, and a post shows me a similar situation.

Re: Not able to connect with MKE15Z using J-Link - NXP Community

I try to erase all pin following the post:

Communication error while accessing MDM-AP. - NXP Community