How I can use CMSIS in S32K Design Studio with S32K148(freeRTOS)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How I can use CMSIS in S32K Design Studio with S32K148(freeRTOS)

3,017 次查看
Learner
Contributor III

Hi 
Is it possible to Integrate CMSIS with S32K Design Studio ?
If yes, Please share me the process to integrate CMSIS with S32K Design Studio.

Thanks 

0 项奖励
回复
2 回复数

2,991 次查看
Learner
Contributor III

Thanks @mikedoidge 
I will go through with the tutorial.

0 项奖励
回复

3,002 次查看
mikedoidge
NXP Employee
NXP Employee

Hello @Learner,

There is a great tutorial on using CMSIS here: https://mcuoneclipse.com/2013/02/14/tutorial-using-the-arm-cmsis-library/

It was written by our colleague @BlackNight. While the device is different and the tool (CodeWarrior) is different, the steps should be quite similar as the devices use ARM cores and the tools are built on Eclipse.

Best Regards,

Mike

0 项奖励
回复