S32K146-100 NxP S32 Studio Examples

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K146-100 NxP S32 Studio Examples

ソリューションへジャンプ
3,944件の閲覧回数
jorgesuarez-riv
Contributor II

It looks that the only hello world example available in S32 Studio for the S32K146 is only for the 144 package. Is this correct? or I'm missing something? How can I change the configuration for the 100 packaging?

s32146-144.PNG

Thanks

1 解決策
3,401件の閲覧回数
raresvasile
NXP Employee
NXP Employee

Hi,

Here you can find the sequence of operations needed to change the CPU count.

https://community.nxp.com/docs/DOC-334936 

Best regards,

Rares

元の投稿で解決策を見る

3 返答(返信)
3,401件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Sorry, I overlooked that you are looking only for package settings. It looks like that even Hello word doesn't support 100 pin package in Beta SDK. I'll clarify this topic with SDK team and let you know. 

Jiri 

0 件の賞賛
返信
3,402件の閲覧回数
raresvasile
NXP Employee
NXP Employee

Hi,

Here you can find the sequence of operations needed to change the CPU count.

https://community.nxp.com/docs/DOC-334936 

Best regards,

Rares

3,401件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

correct - in EAR SDK v0.8.6 is only one S32K146 example. You can use S32K14x Beta SDK v1.9.0 instead - there is full set of examples present: 

pastedImage_2.png

The Beta SDK is part of S32DS update. On main menu bar click on Help -> Install new Software choose all available sites, check what you like to update and pres next button:

pastedImage_3.png

Jiri

0 件の賞賛
返信