S32K146-100 NxP S32 Studio Examples

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K146-100 NxP S32 Studio Examples

跳至解决方案
3,943 次查看
jorgesuarez-riv
Contributor II

It looks that the only hello world example available in S32 Studio for the S32K146 is only for the 144 package. Is this correct? or I'm missing something? How can I change the configuration for the 100 packaging?

s32146-144.PNG

Thanks

1 解答
3,400 次查看
raresvasile
NXP Employee
NXP Employee

Hi,

Here you can find the sequence of operations needed to change the CPU count.

https://community.nxp.com/docs/DOC-334936 

Best regards,

Rares

在原帖中查看解决方案

3 回复数
3,400 次查看
jiri_kral
NXP Employee
NXP Employee

Sorry, I overlooked that you are looking only for package settings. It looks like that even Hello word doesn't support 100 pin package in Beta SDK. I'll clarify this topic with SDK team and let you know. 

Jiri 

0 项奖励
回复
3,401 次查看
raresvasile
NXP Employee
NXP Employee

Hi,

Here you can find the sequence of operations needed to change the CPU count.

https://community.nxp.com/docs/DOC-334936 

Best regards,

Rares

3,400 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

correct - in EAR SDK v0.8.6 is only one S32K146 example. You can use S32K14x Beta SDK v1.9.0 instead - there is full set of examples present: 

pastedImage_2.png

The Beta SDK is part of S32DS update. On main menu bar click on Help -> Install new Software choose all available sites, check what you like to update and pres next button:

pastedImage_3.png

Jiri

0 项奖励
回复