S32G274A - HUGE blob file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G274A - HUGE blob file

ソリューションへジャンプ
1,527件の閲覧回数
ofer-bahar-guardknox
Contributor IV

working on S32DS 3.5 , RTD 4.0.1 on the GOLDBOX (RDB2)

Starting from NXP example project Dio_ToggleLed_S32G274A_M7, the project runs perfect

followed the steps in : https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Use-IVT-Tool-To-Create-A-Blob-Im...

Built and created the bin file, also created the DCD file

when exporting blob file, its 875MB !!!

Of coarse can't be written to flashed and the flash tool says its too large 

oferbaharguardknox_0-1688557833434.png

in the IVT tool everything looks perfect  

oferbaharguardknox_1-1688557909832.png

the size of the image looks OK, all else as well 

What is wrong here? 

Why is the blob file so large?

0 件の賞賛
返信
1 解決策
1,520件の閲覧回数
ofer-bahar-guardknox
Contributor IV

The problem is that in the Application bootloader section, before exporting blob file, the image file should be selected as the one from the Generated image file (aka the full application image file) => VERY CONFUSING , and un associative

(instead of put it in the UI in a place that the user can understand that it should be selected)

 Anyway when selecting the 'generated image file' - everything is OK and the FLASH is written OK 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,521件の閲覧回数
ofer-bahar-guardknox
Contributor IV

The problem is that in the Application bootloader section, before exporting blob file, the image file should be selected as the one from the Generated image file (aka the full application image file) => VERY CONFUSING , and un associative

(instead of put it in the UI in a place that the user can understand that it should be selected)

 Anyway when selecting the 'generated image file' - everything is OK and the FLASH is written OK 

0 件の賞賛
返信