S32G2: S32DS: Cannot open the Configuration Tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G2: S32DS: Cannot open the Configuration Tool

Jump to solution
6,498 Views
Keita_Nagashima
NXP Employee
NXP Employee

Hi Sir or Madam,

I installed necessary packages into S32DS, and imported some example projects.

KeitaNaga_1-1647313925418.pngKeitaNaga_1-1647313925418.png

Some projects can be installed into my environment, but the .mek file for Configuration Tool cannot be opened.

KeitaNaga_2-1647314392744.pngKeitaNaga_2-1647314392744.png

 

This issue appears to depend on PlatformSDK version, but I couldn't understand the version dependence.

 

Would you tell me the how to solve this issue? 

I would also like to know about the Version dependency with PlatformSDK.

 

Best Regards,

Keita

 

 

0 Kudos
Reply
1 Solution
6,484 Views
mikedoidge
NXP Employee
NXP Employee

Hello Keita,

It seems this project is quite old and was created for the RTD which was released in December 2020. I suggest you use the new version which was included in the updated RTD you installed.

image.pngimage.png

Best Regards,

Mike

View solution in original post

0 Kudos
Reply
6 Replies
6,485 Views
mikedoidge
NXP Employee
NXP Employee

Hello Keita,

It seems this project is quite old and was created for the RTD which was released in December 2020. I suggest you use the new version which was included in the updated RTD you installed.

image.pngimage.png

Best Regards,

Mike

0 Kudos
Reply
6,474 Views
Keita_Nagashima
NXP Employee
NXP Employee

@mikedoidge ,

 

Thank you for your reply. I understood it.

BTW, do you know how to delete the old project like December 2020 version?

I'd like to manage the all project.

 

Best Regards,

Keita

0 Kudos
Reply
6,459 Views
mikedoidge
NXP Employee
NXP Employee

Hello Keita,

To remove the old examples, you would need to uninstall the old RTD. Probably it is the 2.0.0 version.

image.pngimage.png

 

0 Kudos
Reply
6,452 Views
Keita_Nagashima
NXP Employee
NXP Employee

Hi @mikedoidge ,

Thank you for your reply.

Please refer to the figure in my original message. I have already deleted the old RTD and my environment was not seen it.

But, the old version of the sample programs are still there...

 

Best Regards,

Keita

0 Kudos
Reply
6,421 Views
mikedoidge
NXP Employee
NXP Employee

If the old version of the RTD was uninstalled from S32 Design Studio, then the associated example projects should be removed as part of that process.

Perhaps check the following directories to see if some content from the old RTD is left behind:

C:\NXP\S32DS.3.4\S32DS\integration

C:\NXP\S32DS.3.4\S32DS\software

Best Regards,

Mike

0 Kudos
Reply
6,367 Views
Keita_Nagashima
NXP Employee
NXP Employee

Hi @mikedoidge ,

 

Sorry for my delay response.

Yes, I was able to remove old sample codes by deleting the old files manually.

 

Best Regards,

Keita

0 Kudos
Reply