S32G How to configure CODE memory region to store executable program.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G How to configure CODE memory region to store executable program.

4,481 Views
vinod_bargaje
Contributor II

Hi,

I am using S32G part and I have few queries related to usage of memory section of S32G274A,

- S32G274A memory section contains CODE region and Ram Region 

- code section starts with  0x00_0000_0000 to 0x00_1FFF_FFFF

- Ram section range : 0x00_2000_0000 to 0x00_3FFF_FFFF

We have sample code that stores code in to RAM region.  

how we can use CODE section for for storing executable code. Any Linker configuration that we need to do?

Any sample code reference would help! 

Thannks in advance. 

0 Kudos
Reply
4 Replies

4,299 Views
yihan_cheng
Contributor II

Could you send me a SD card bootable Image, that you build with IVT Tools. It will be very nice of you, if you could also explain briefly like each part of those Image.

My email address: [email protected]

BR.
Yihan

0 Kudos
Reply

4,299 Views
yihan_cheng
Contributor II

Hi [email protected]

Recently I try to build the bootloader image for s32g274aevb. I would like to ask if you have the experience to build the Image Table with IVT configuration tools?

Thanks

Yihan Cheng

0 Kudos
Reply

4,299 Views
vinod_bargaje
Contributor II

hi [email protected]‌ 

I am able to build image with IVT configuration tools.

Let me know if you need any specific support for same. 

0 Kudos
Reply

4,299 Views
andrei_skok
NXP Employee
NXP Employee

I see your open service request #00260255 with the same question assigned to our S32G Application team.

Please wait their answer to that Request.

0 Kudos
Reply