S32G How to configure CODE memory region to store executable program.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32G How to configure CODE memory region to store executable program.

4,444 次查看
vinod_bargaje
Contributor II

Hi,

I am using S32G part and I have few queries related to usage of memory section of S32G274A,

- S32G274A memory section contains CODE region and Ram Region 

- code section starts with  0x00_0000_0000 to 0x00_1FFF_FFFF

- Ram section range : 0x00_2000_0000 to 0x00_3FFF_FFFF

We have sample code that stores code in to RAM region.  

how we can use CODE section for for storing executable code. Any Linker configuration that we need to do?

Any sample code reference would help! 

Thannks in advance. 

0 项奖励
回复
4 回复数

4,262 次查看
yihan_cheng
Contributor II

Could you send me a SD card bootable Image, that you build with IVT Tools. It will be very nice of you, if you could also explain briefly like each part of those Image.

My email address: [email protected]

BR.
Yihan

0 项奖励
回复

4,262 次查看
yihan_cheng
Contributor II

Hi [email protected]

Recently I try to build the bootloader image for s32g274aevb. I would like to ask if you have the experience to build the Image Table with IVT configuration tools?

Thanks

Yihan Cheng

0 项奖励
回复

4,262 次查看
vinod_bargaje
Contributor II

hi [email protected]‌ 

I am able to build image with IVT configuration tools.

Let me know if you need any specific support for same. 

0 项奖励
回复

4,262 次查看
andrei_skok
NXP Employee
NXP Employee

I see your open service request #00260255 with the same question assigned to our S32G Application team.

Please wait their answer to that Request.

0 项奖励
回复