S32DS3.4/3.5_Blue Screen Issue_FC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS3.4/3.5_Blue Screen Issue_FC

1,918 Views
Fidel
Contributor IV

Dears,

       Recently , I met an boring issue when using S32DS to develop S32K, when I compile the program , PC sometimes became blue screen , I tried the version 3.4 and 3.5, both  have the same issue , and it randomly happend, my colleages also install the same version with the same version of Windows OS and patchs. but it is ok on his PC, and fail on my PC, the issue picture as below , anyone can tell me what happened and how to resolve it? thanks a lot~

Fidel_0-1668429505590.pngFidel_0-1668429505590.png

 

0 Kudos
Reply
4 Replies

1,906 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

it is probably some HW issue with your PC - bad memory? Or something else. 

 

Jiri 

0 Kudos
Reply

1,904 Views
Fidel
Contributor IV

Is it possible that the S32DS software is not compatible with the Windows OS ?

0 Kudos
Reply

1,901 Views
jiri_kral
NXP Employee
NXP Employee

Hi,

not, it is not possible. To be honest - this is the very first time when I saw BSOD in relation with S32DS. As you said - your colleague is not facing this issue with the same configuration. 

Try to check your HW - the Memory/Clock settings in BIOS is the most common source of BSOD. 

0 Kudos
Reply

1,898 Views
Fidel
Contributor IV

OK , I will try that ,thanks  a lot~

0 Kudos
Reply