S32DS v3.2 installation fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS v3.2 installation fail

ソリューションへジャンプ
8,275件の閲覧回数
shuyaizumikawa
Contributor II

Hi, Dear community member

I am trying to install S32DS v3.2 on my windows-10 PC, but my activation code is probably incorrect and appear to pop up message as following, eventually cannot complete install S32DS3.2.

"Software Acticvation Code is already used on this station for S32DS_3.2 APU3Compiler 1.0"

As my test, I also download S32DS v3.2 exe file for multiple times from NXP.com, but new activation code did not issue and did not receive via its related e-mail, so I couldn't try new activation code.

First of all, please can you advise what I should do for above pop-up messages or its meanings ?

Please see attached setup procedures that I tried.

Best regards

SHUYA IZUMIKAWA

0 件の賞賛
返信
1 解決策
8,099件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Note to community: We have resolved this issue by the following via a separate support communication method:

The installer has identified a conflict with another installation using a similar license on the same PC. This could be an issue with the trusted storage. Please try the following:

-> Delete 'C:\ProgramData\FLEXNet'

This folder may be hidden by default, so then it would be necessary to change Windows Explorer settings to show hidden items.

After this, try to install again. The installation should be able to complete.

We received confirmation that this solved the issue from Shuya Izumikawa's colleague.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
8,100件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Note to community: We have resolved this issue by the following via a separate support communication method:

The installer has identified a conflict with another installation using a similar license on the same PC. This could be an issue with the trusted storage. Please try the following:

-> Delete 'C:\ProgramData\FLEXNet'

This folder may be hidden by default, so then it would be necessary to change Windows Explorer settings to show hidden items.

After this, try to install again. The installation should be able to complete.

We received confirmation that this solved the issue from Shuya Izumikawa's colleague.

0 件の賞賛
返信
7,034件の閲覧回数
zxd1
Contributor I
this method is no use
0 件の賞賛
返信
7,041件の閲覧回数
zxd1
Contributor I

i have follow you advise steps to operator, but the problem is still apprear, i have seach answer on the internet but i have not found any tips

0 件の賞賛
返信