S32DS for Power issue: lib_c99.prefix No such file or directory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32DS for Power issue: lib_c99.prefix No such file or directory

3,129 次查看
momo
NXP Employee
NXP Employee

Hi:

I'm developing MPC5748G project with S32DS for Power, when I add some code in the project, there's an error reported:

lib_c99.prefix: No such file  or directory.

Do you know how to fix this issue? Thank you

2 回复数

2,244 次查看
StephenDu
NXP Employee
NXP Employee

You can try to change the library from EWL to newlib when you create project. you also can change this setting after you create project. PATH: Project right click --> Propertites --> C/C++ Build --> Settings --> Target Processor --> Libraries support.

I don't know the root cause, but i meet the same problem and solved by changing the library setting.

0 项奖励
回复

2,244 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please share more details? Description that you added "some code" is not enough to provide any support. It will be best, if you can share some simple example, which demonstrates your problem. If this is not possible, please provide as much details as possible.

Regards,

Martin