S32DS debug error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32DS debug error

跳至解决方案
2,718 次查看
海波张
Contributor I

Error in services launch sequence
Failed to launch GDB server. Please check that another instance of pegdbserver_console.exe is not running.

How to solve the problem, thank you!

标记 (2)
0 项奖励
回复
1 解答
2,431 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

just check if another GDB server is not running via task manager. In windows press CTRL+SHIFT+ESC to start task manager. If there is present pegdbserver process - just kill it. It may happen if for example debug session is interrupted by disconnect from USB or power outage.

Jiri

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,431 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

See the answer from Jiri (find and kill the P&E gdb server in the task manager). Otherwise, this article shows it for KDS, but the same principle applies to S32 DS.

Erich

0 项奖励
回复
2,432 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

just check if another GDB server is not running via task manager. In windows press CTRL+SHIFT+ESC to start task manager. If there is present pegdbserver process - just kill it. It may happen if for example debug session is interrupted by disconnect from USB or power outage.

Jiri

0 项奖励
回复