S32DS debug error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS debug error

Jump to solution
2,706 Views
海波张
Contributor I

Error in services launch sequence
Failed to launch GDB server. Please check that another instance of pegdbserver_console.exe is not running.

How to solve the problem, thank you!

Tags (2)
0 Kudos
Reply
1 Solution
2,419 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

just check if another GDB server is not running via task manager. In windows press CTRL+SHIFT+ESC to start task manager. If there is present pegdbserver process - just kill it. It may happen if for example debug session is interrupted by disconnect from USB or power outage.

Jiri

View solution in original post

0 Kudos
Reply
2 Replies
2,419 Views
BlackNight
NXP Employee
NXP Employee

Hello,

See the answer from Jiri (find and kill the P&E gdb server in the task manager). Otherwise, this article shows it for KDS, but the same principle applies to S32 DS.

Erich

0 Kudos
Reply
2,420 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

just check if another GDB server is not running via task manager. In windows press CTRL+SHIFT+ESC to start task manager. If there is present pegdbserver process - just kill it. It may happen if for example debug session is interrupted by disconnect from USB or power outage.

Jiri

0 Kudos
Reply