S32DS debug error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
7,724件の閲覧回数
George_Ye
Contributor II

I used to debug with version 3.4.0 normally. Today, after updating with the 3.4.3 update package, an error occurred. Tips "Break at address "0x0" with no debug information available, or outside of program code",how can I do?

My debugger is PE micro.

ラベル(1)
0 件の賞賛
返信
1 解決策
7,382件の閲覧回数
George_Ye
Contributor II
配置工具和SDK不配套

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
7,392件の閲覧回数
hupengpeng203
Contributor I

我和你有同样的问题。你解决了吗?

0 件の賞賛
返信
7,382件の閲覧回数
George_Ye
Contributor II
配置工具和SDK不配套
0 件の賞賛
返信
7,709件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

what's your target MCU? Can you please share output from debug console? What optimization level - is set do none? 

0 件の賞賛
返信
7,695件の閲覧回数
George_Ye
Contributor II

See attach file, thanks.MCU is s32k 314.optimization level is "-Os"(Optimize for size), and setting to none also made no sense.

0 件の賞賛
返信