Connection from "127.0.0.1" via 127.0.0.1. Connection from port "51177" to 6224 Connection from "127.0.0.1" via 127.0.0.1. Connection from port "51190" to 7224 Telnet server running on 127.0.0.1:51794 Searching for Kernel Symbols... rsp_qC - qSymbol: 5F74785F7468726561645F63757272656E745F707472 _tx_thread_current_ptr not found. ThreadX analysis not enabled. rsp_qC - qSymbol: 707843757272656E74544342 pxCurrentTCB not found. FreeRTOS analysis not enabled. Unable to load libusb0.dll Copyright 2021 P&E Microcomputer Systems,Inc. Command Line :C:\NXP\S32DS.3.4\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_5.1.7.202112141853\win32\pegdbserver_console -device=NXP_S32K3xx_S32K314 -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=5000 -port=U? PEmicro Interface detected - Flash Version 10.84 CMD>RE Initializing. Soft reset failed! Target has been RESET and is active. CMD>CM C:\NXP\S32DS.3.4\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_5.1.7.202112141853\win32\gdi\P&E\supportFiles_ARM\NXP\S32K3xx\nxp_s32k314_1x32x1012k_hse_disabled.arp Initializing. Soft reset failed! Initialized. ;version 1.00, 09/03/2021, Copyright 2021 P&E Microcomputer Systems, www.pemicro.com [S32K3x4_hse_disabled] ;device nxp, s32k314, 1x32x1012k,desc=hse_disabled ;begin_cs device=$00400000, length=$003F4000, ram=$20400000 Loading programming algorithm ... WARNING - Selected .ARP file has been modified. CRC16 = $7E41 Done. Programming sequency is : erase, blank check, program, and verify {default} CMD>VC Command is inactive for this .ARP file. VC is not implemented, falling back to VM CMD>VM Verifying. Verified. Application verified in memory. No need to reprogram. CMD>RE Initializing. Soft reset failed! Target has been RESET and is active. Soft reset failed! Starting reset script (C:\NXP\S32DS.3.4\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_5.1.7.202112141853\win32\gdi\P&E\supportFiles_ARM\NXP\S32K3xx\S32K314.mac) ... REM Enable clocks for selected cores in MC_ME module (the sequence below enables all clocks). REM Initialize RAM and DMA: REM Initialize DMA TCD: REM Copy valid executable code to RAM for each core to be used. REM Enable required cores in MC_ME: Delaying for 20mS ... Done. Reset script (C:\NXP\S32DS.3.4\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_5.1.7.202112141853\win32\gdi\P&E\supportFiles_ARM\NXP\S32K3xx\S32K314.mac) completed. BusFault: An imprecise (asynchronous) data access error has occurred. HardFault: A fault has been escalated to a hard fault.