S32DS Vision:Segmentation fault

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS Vision:Segmentation fault

Jump to solution
3,013 Views
liujinbao
Contributor II

hello:

I use the board SBC_S32V234.

The BSP version I am using is VisionSDK_S32V2_RTM_1_3_0_img_yocto.

On the official website,the file name is as follows (yellow box):

pastedImage_1.png
S32DS_Vision_v2.0 is installed on windows7 64.
After I compiled isp_sonyimx224_sci_dcu:A53_Linux, the generated executable file was sent to the development board via SSH, and the execution failed, as shown below:

1.png

0 Kudos
Reply
1 Solution
2,903 Views
liujinbao
Contributor II

After replacing S32DS_Vision_v2.0 with S32DS_Vision_2018.R1, the routine can be executed normally.

1.png

thanks!

View solution in original post

0 Kudos
Reply
2 Replies
2,903 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

S32DS for Vision v2.0 contains VSDK RTM v1.0.0. Some examples aren't compatible with OS image from VSDK RTM v1.3.0. Please use OS image which comes with S32DS Installation. 

Or you can use new S32DS - https://community.nxp.com/docs/DOC-342080

Jiri 

0 Kudos
Reply
2,904 Views
liujinbao
Contributor II

After replacing S32DS_Vision_v2.0 with S32DS_Vision_2018.R1, the routine can be executed normally.

1.png

thanks!

0 Kudos
Reply