S32DS Vision:Segmentation fault

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS Vision:Segmentation fault

ソリューションへジャンプ
2,939件の閲覧回数
liujinbao
Contributor II

hello:

I use the board SBC_S32V234.

The BSP version I am using is VisionSDK_S32V2_RTM_1_3_0_img_yocto.

On the official website,the file name is as follows (yellow box):

pastedImage_1.png
S32DS_Vision_v2.0 is installed on windows7 64.
After I compiled isp_sonyimx224_sci_dcu:A53_Linux, the generated executable file was sent to the development board via SSH, and the execution failed, as shown below:

1.png

0 件の賞賛
返信
1 解決策
2,829件の閲覧回数
liujinbao
Contributor II

After replacing S32DS_Vision_v2.0 with S32DS_Vision_2018.R1, the routine can be executed normally.

1.png

thanks!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,829件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

S32DS for Vision v2.0 contains VSDK RTM v1.0.0. Some examples aren't compatible with OS image from VSDK RTM v1.3.0. Please use OS image which comes with S32DS Installation. 

Or you can use new S32DS - https://community.nxp.com/docs/DOC-342080

Jiri 

0 件の賞賛
返信
2,830件の閲覧回数
liujinbao
Contributor II

After replacing S32DS_Vision_v2.0 with S32DS_Vision_2018.R1, the routine can be executed normally.

1.png

thanks!

0 件の賞賛
返信