S32DS V3.5 on WSL needs daily Re-Activation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32DS V3.5 on WSL needs daily Re-Activation

跳至解决方案
2,350 次查看
scheuch-heilig
Contributor I

I have installed S32DS V3.5 (Linux) on my WSL(2) image.

Every day I start WSL / S32DS new it prompts with Activation dialogue and message "License missing"

2023-10-04_09h48_29.png

Activation (offline) does work correctly with request.xml and activation.xml, but it is very annoying to do this on a daily basis.

The different versions of request.xml appear to vary in the parameter 'UniqueMachineNumber'

Thank you for any help to solve this.

 

0 项奖励
回复
1 解答
2,314 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @scheuch-heilig , 

 

As you pointed out, the different versions of request.xml appear to vary in the parameter 'UniqueMachineNumber' because of using non-persistent Virtual machine. 

 

The license is attached to the Machine - computer system, because of that you are required to activate daily. 

 

May be can you contact if you can get persistent VM, or if you can directly use on Linux. 

 

Please let me know if any further question. 

 

Thank you. Kind regards.

 

-Mehul Patel

在原帖中查看解决方案

0 项奖励
回复
8 回复数
1,995 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @scheuch-heilig , 

I see the S32DS 3.5 is activated, the issue was resolved right. 

Thank you. Best regards, 

- Mehul Patel 

1,984 次查看
scheuch-heilig
Contributor I
Hello Mehul,

The problem is still the same, but I have switched to a different IDE environment.
So I don't need S32DS on my VM any more.

You can close this issue if you like

Thanks for your efforts
Best regards
0 项奖励
回复
2,218 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @scheuch-heilig , 

 

Is the issue has been solved? 

 

Please let us know any further update on the issue. 

 

Thank you. Best regards, 

 

-Mehul Patel 

0 项奖励
回复
2,204 次查看
scheuch-heilig
Contributor I

Hi Mehul,

Here is the Activation code: 45FB-E7C4-2E77-CF8F

And the installation log attached.

 

Best Regards

@scheuch-heilig 

0 项奖励
回复
2,315 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @scheuch-heilig , 

 

As you pointed out, the different versions of request.xml appear to vary in the parameter 'UniqueMachineNumber' because of using non-persistent Virtual machine. 

 

The license is attached to the Machine - computer system, because of that you are required to activate daily. 

 

May be can you contact if you can get persistent VM, or if you can directly use on Linux. 

 

Please let me know if any further question. 

 

Thank you. Kind regards.

 

-Mehul Patel

0 项奖励
回复
2,262 次查看
scheuch-heilig
Contributor I

Thank you for the explanation.

I have checked the machine-id (/var/lib/dbus/machine-id) on various starts of my WSL environment.

The reported machine id always persistently stays the same.
This is, even if I restart the PC, so the VM (WSL) appears to be persistent

Looks like there are more parameters used for this license check

0 项奖励
回复
2,235 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @scheuch-heilig , 

Please can you share your activation code for the S32DS, to check the problem. 

 

Also please can you share log from 

 

C:\NXP\S32DS.3.5\_S32 Design Studio for S32 Platform 3.5_installation\Logs

 

(or wherever S32DS is located) 

 

Thank you. Best regards. 

-Mehul Patel

0 项奖励
回复
2,190 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @scheuch-heilig , 

 

As I see activation transactions using your activation code, there is different unique machine ID in the different activation request . 

 

Please can you check with your company's It team, why is it so? 

 

Thank you. Best regards. 

 

- Mehul Patel 

 

 

0 项奖励
回复