S32DS Stop at launching debugger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS Stop at launching debugger

3,698 Views
alex_yu1
Contributor III

hello,

     i have import a FLASH example. The S32 DS can not enter the debug perspective, it stop at the launching : initializing debugger services. Sources_main.c - S32 Design Studio for ARM.png

Labels (1)
3 Replies

3,295 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

how do you connect your board? Do you use OpenSDA or some debug probe?

What is the mask of the microcontroller you try to connect?

Have you correctly installed PEMicro drivers? Please look at the thread below

https://community.nxp.com/thread/447395 

Regards,

Martin

0 Kudos
Reply

3,295 Views
alex_yu1
Contributor III

i make it after killing some security process of PC

3,295 Views
alex_yu1
Contributor III

hello martin,

       I connect the board by the USB with openSDA.

The mask is PS32K144HFVLL 0N77P QAF1612A on the micro-p

I have installed the PEMicro drivers. PC can find the openSDA in the device manager.

Thanks and regards

Alex

0 Kudos
Reply