S32DS Stop at launching debugger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS Stop at launching debugger

3,664件の閲覧回数
alex_yu1
Contributor III

hello,

     i have import a FLASH example. The S32 DS can not enter the debug perspective, it stop at the launching : initializing debugger services. Sources_main.c - S32 Design Studio for ARM.png

ラベル(1)
タグ(3)
3 返答(返信)

3,261件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

how do you connect your board? Do you use OpenSDA or some debug probe?

What is the mask of the microcontroller you try to connect?

Have you correctly installed PEMicro drivers? Please look at the thread below

https://community.nxp.com/thread/447395 

Regards,

Martin

0 件の賞賛
返信

3,261件の閲覧回数
alex_yu1
Contributor III

i make it after killing some security process of PC

3,261件の閲覧回数
alex_yu1
Contributor III

hello martin,

       I connect the board by the USB with openSDA.

The mask is PS32K144HFVLL 0N77P QAF1612A on the micro-p

I have installed the PEMicro drivers. PC can find the openSDA in the device manager.

Thanks and regards

Alex

0 件の賞賛
返信