S32DS - S32K3 SDK error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS - S32K3 SDK error

Jump to solution
9,176 Views
matej_15
Contributor III

Hi, 

 

I get the following error while trying to open the pins wizard:

matej_15_0-1666008031403.png

 

I have S32 Design Studio for S32 Platform, Version: 3.5 installed together with the following extensions:

matej_15_1-1666008114485.png

matej_15_2-1666008124236.png

 

I have seen similar errors regarding S32K1 and theirs solution suggested to download SDK and install it offline, but I can't seem to find the S32K3_2022_03 SDK on S32DS website. Can you please provide us with help so we can open this project?

 

Br,

0 Kudos
Reply
1 Solution
9,165 Views
mikedoidge
NXP Employee
NXP Employee

Hello @matej_15,

Please login to your account and proceed all the way until you reach the Product List page. Then try this link: https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=13397517

Download the file: SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204.zip  this matches the version shown in the error message. 

I see from the release notes that S32 Design Studio v3.4 Update 3 is supported. So you may need to have S32DS 3.4 installed with Update 3 and no later updates. If you have already installed Update 4 or it forces you to install Update 4, you can try it, but if you still get an error, then try with a fresh install of v3.4 and Update 3. You may need to download the Update 3 and disable the S32DS online update site to prevent it from seeing Update 4.

Best Regards,

Mike

View solution in original post

4 Replies
8,989 Views
strauserj
Contributor I

Hello, I'm looking for SDK and RTD for S32K3. The download link above is no longer valid. Can you provide a new link all update packages for S32K344 board?

Thank you, Jason

0 Kudos
Reply
8,970 Views
mikedoidge
NXP Employee
NXP Employee

Hi Jason,

Login to your software account at NXP.com, proceed until you reach the Product List page. Next, select the product 'Automotive SW - S32K3 Standard Software'. From there you'll find the S32K344 RTD packages for S32 Design Studio within 'Automotive SW - S32K3 - Real-Time Drivers for Cortex-M'. There's several packages listed, some are for other S32K3 family devices. The latest RTD for S32K344 is 'S32K3 Real-Time Drivers Version 2.0.3' published on Feb 17, 2023. The S32DS integration package is the one with 'DS_updatesite' in the name and suffix '.ZIP'.

Best Regards,

Mike

5,198 Views
AbhishekK
Contributor III

AbhishekK_0-1739797455444.png

 

I have used this S32DS 3.4 update 3 and  RTD package as mentioned . but still facing the error .

AbhishekK_2-1739797959484.png

 

I am try to build this Examples 

AbhishekK_1-1739797813544.png

 

 

 

 

0 Kudos
Reply
9,166 Views
mikedoidge
NXP Employee
NXP Employee

Hello @matej_15,

Please login to your account and proceed all the way until you reach the Product List page. Then try this link: https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=13397517

Download the file: SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204.zip  this matches the version shown in the error message. 

I see from the release notes that S32 Design Studio v3.4 Update 3 is supported. So you may need to have S32DS 3.4 installed with Update 3 and no later updates. If you have already installed Update 4 or it forces you to install Update 4, you can try it, but if you still get an error, then try with a fresh install of v3.4 and Update 3. You may need to download the Update 3 and disable the S32DS online update site to prevent it from seeing Update 4.

Best Regards,

Mike