S32DS Processor Selection Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS Processor Selection Problem

11,002 Views
yunus_ozdemir
Contributor I

Hello,

 

I am newbie on S32DS. I am trying to create a new project like File -> New -> New S32DS Project. I couldn't see processors. Something installed wrong way or not installed yet? Waiting for your help.

 

Thanks in advance

Yunus.150066_150066.JPGS32DS_image.JPG

0 Kudos
Reply
15 Replies

10,072 Views
yunus_ozdemir
Contributor I

Hello Stan,

What about eclipse file research by your side? Did you catch the problem?

Thank you,

Yunus.

0 Kudos
Reply

10,072 Views
stanish
NXP Employee
NXP Employee

Yunus,

Specifically for KEA there are multiple choices. It's supported by both CodeWarrior for MCUs 10.6 and KDS There is also a standalone flasher available for programming by pemicro:

P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools...

Regards,

Stan

0 Kudos
Reply

10,072 Views
yunus_ozdemir
Contributor I

Hello Stan,

Thank you for your fast reply. Waiting the result of development team.

I got one more question that out of this topic. Which program should I use for programming KEA family processor via U-Multilink? Is there any programming enviroment except S32DS IDE?

Regards,

Yunus.

0 Kudos
Reply

10,072 Views
vinithabm
Contributor II

Hello Yunus,

Did you find the reason to the question?

I am also facing the same issue. 

Can you please let m know how did you solve this issue?

Thank you,

Vinitha

0 Kudos
Reply

10,072 Views
yunus_ozdemir
Contributor I

Hi Vinitha,

Unfortunately, i could not solve the problem. I decided to use Codewarrior.

Yunus

0 Kudos
Reply

10,072 Views
vinithabm
Contributor II

Hello Yunus,

I got to know the solution.

I need to install S32 Design Studio for Power Architecture IDE, (not S32 Design Studio ARM) that supports MPC5748G controller.

Power Architecture IDE, they are releasing within a week.

Thank you for the alternative option, Codewarrior.

Best,

Vinitha

0 Kudos
Reply

10,072 Views
stanish
NXP Employee
NXP Employee

Hello Yunus,

Thanks for the update.

Regarding system requirements - it's mentioned in the release notes (c:\Freescale\S32_ARM_v1.2\S32DS\Release_Notes\Release_Notes.pdf). See the snippet below.

Anyway in your case I suspect the issue might be caused by an interference with another application/program.

I've informed our development team about the issue so the investigation is in progress.

Stan

3 System Requirements

3.1 Recommended Configuration

 2.6GHz Pentium® compatible processor or better

 4GB RAM

 2GB

 400MB on Windows system disk

 USB port for communications with target hardware

 Ethernet port for communications with target hardware (optional)

3.2 Operational Minimum Configuration

 1.8GHz Pentium® compatible processor or better

 2GB RAM

 2GB

 400MB on Windows system disk

 USB port for communications with target hardware

3.3 Host Operating System Support

 Microsoft Windows 7 32-bit and 64-bit (Home Premium Edition and Professional Edition)

 Microsoft Windows 8 32-bit and 64-bit (Home Premium Edition and Professional Edition)

 Microsoft Windows 8.1 32-bit and 64-bit (Home Premium Edition and Professional Edition)

 Microsoft Windows 10 32-bit and 64-bit (Home and Pro Editions)

0 Kudos
Reply

10,072 Views
yunus_ozdemir
Contributor I

Hi Stan,

I have tried to work with another machine and seems same result. Could you please share system requirements of S32DS?

Also, I am sharing the eclipse file with two parts in below.

http://www.megafileupload.com/rVlT/eclipse.zip.001

http://www.megafileupload.com/jx4u/eclipse.zip.002

Waiting news!

Yunus

0 Kudos
Reply

10,072 Views
stanish
NXP Employee
NXP Employee

Hi Yunus,

It seems that something wrong happened during installation.

Could you possibly try to re-install and reboot? Do you have any other machine you can test it with?

If it does not help - could you send us entire zipped eclipse directory (~500MB).

Thanks a lot for your cooperation!

Regards,

Stan

0 Kudos
Reply

10,072 Views
yunus_ozdemir
Contributor I

It doesn't work, same problem appeared...

0 Kudos
Reply

10,072 Views
stanish
NXP Employee
NXP Employee

When you start S32DS IDE it asks you to enter a workspace directory:

pastedImage_0.png

So if you add a new folder which doesn't exist yet it creates a blank new workspace for you.

S.

0 Kudos
Reply

10,072 Views
yunus_ozdemir
Contributor I

Hi Stan,

How do i create a new clean workspace?

Yunus.

0 Kudos
Reply

10,072 Views
stanish
NXP Employee
NXP Employee

Hi,

One more comment:

Could you try to use a new clean workspace?

S.

0 Kudos
Reply

10,072 Views
yunus_ozdemir
Contributor I

Hi Stan,

Thank you for your interest. I attached the log file below. My OS is Windows 7 professional.

http://www.megafileupload.com/fbpz/log​

Yunus

0 Kudos
Reply

10,072 Views
stanish
NXP Employee
NXP Employee

Hi Yunus,

Could you possibly attach  your .log located in <workspace>\.metadata?

Which OS do you use?

This may help us to identify what is wrong.

Thanks.

Stan

0 Kudos
Reply