S32DS, MPC5777C and PIT interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32DS, MPC5777C and PIT interrupt

2,475 次查看
robertfromcummi
Contributor II

I try to use PEmicro with MPC5777C on S32DS and I cannot generate interrupt from PIT when in debug mode. What should I check?

标签 (2)
0 项奖励
回复
2 回复数

1,914 次查看
stanish
NXP Employee
NXP Employee

Robert ,

FYI: This is a known issue with PIT freeze mode bit (ENGR00379206).

When there is a freeze mode activated the debug run does not trigger start of a timer/peripheral.

Please disable freeze bit as a workaround.

This issue should be addressed in a next release.

Stan

0 项奖励
回复

1,914 次查看
stanish
NXP Employee
NXP Employee

Hello Robert,

I'd recommend you to download and check PinToggleStationery for MPC5777M since it includes PIT interrupt.

Example MPC5777M PinToggleStationery S32DS

Stan

0 项奖励
回复