S32DS Interface configuration problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS Interface configuration problem

1,377 Views
QJ_HAPPY
Contributor I

Hello:

        I found in the configuration software project that I cannot set "Properties ->Resource ->Linked Resources" in a project in S32DS, as shown in the following figure. How can I set it?

QJ_HAPPY_0-1668579456905.pngQJ_HAPPY_0-1668579456905.png

 

0 Kudos
Reply
1 Reply

1,361 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

This page will display files which have been added to your project as a linked resource. You can set this at the time the files are added. For example, the following menu appears when you drag and drop a file into your project (Project Explorer panel):

mikedoidge_0-1669926195460.pngmikedoidge_0-1669926195460.png

You can see there is an option 'Link to files'. After you add the file, it will appear in the view you shared.

Best Regards,

Mike

0 Kudos
Reply