S32DS For Power v1.1 Debug problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS For Power v1.1 Debug problem

3,346件の閲覧回数
eautopower
Contributor IV

There is a error,like:

pastedImage_1.png

I have already reloade  the S32DS ,but the problem remains unsolved.

please tell me what can I do?

0 件の賞賛
返信
5 返答(返信)

3,038件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello,

I'd strongly recommend you to install the latest version of S32DS for Power v1.2 + updates.

Please check the announcements below:

S32 Design Studio for Power v1.2 (Windows/Linux) released! 

https://community.nxp.com/docs/DOC-335067 

Is this still the problem?

Regards,

Stan

0 件の賞賛
返信

3,038件の閲覧回数
eautopower
Contributor IV

hello,

yes,this is still the problem.

0 件の賞賛
返信

3,038件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

This is Pemicro GDB server crash. It seems there is an interference with another process. Could you possibly try to run GDB server in standalone mode. Let's assume you have S32R274 target.

Run GDB server:

<S32DS_Power_v1.2>\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.6.9.201706282002\win32\pegdbserver_power_console.exe -startserver -device=S32R274 

you should observe something like this:

pastedImage_282.png

Are you able to start GDB server without IDE on your side?

0 件の賞賛
返信

3,038件の閲覧回数
eautopower
Contributor IV

Incompatible with the WIN10 X64 system,it is ok now

0 件の賞賛
返信

3,038件の閲覧回数
eautopower
Contributor IV

Hi:

 I tried to turn it on, but exit quickly when it started running

0 件の賞賛
返信