S32DS For Power Architecture

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS For Power Architecture

2,103件の閲覧回数
kmh48301
Contributor IV

Hello.

I need to use S32DS For Power Architecture IDE and M(S)PC 5775E MCU

And I need to make Library File (.a file) for it with GHS Compiler.

So i have installed and imported the GHS Compiler to S32DS For Power Architecture.

 

But I can't make Library File.

kmh48301_0-1655952402917.png

I can't see the GHS Toolchain in the selection bar.

 

when i create application project, i can see it.

kmh48301_1-1655952469038.png

 

 

Can you please give me a little hand?

I've already asked to my compiler vendor.

But he told me to ask to NXP.

 

Thanks.

Best Regards.

Phillip.

0 件の賞賛
返信
1 返信

2,058件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @kmh48301,

First, use the wizard to create an application project, selecting GHS as the toolchain, then follow the steps in the attached document.

Best Regards,

Mike

0 件の賞賛
返信