S32DS 3.6 on Ubuntu codegen fails - "TypeError: Cannot read property "getName" from undefined"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS 3.6 on Ubuntu codegen fails - "TypeError: Cannot read property "getName" from undefined"

1,177件の閲覧回数
dustinr
Contributor I

This is on S32DS 3.6 on Ubuntu with S32G274A_Rev2, trying to do codegen from a known good .mex file generated in S32DS 3.5.

In text for searchability:

 

 

TypeError: Cannot read property "getName" from undefined
	at Clock_Ip_Cfg_Def_H (clock_utils.js:2500)
	at <anonymous> (<function>:9)
	at generate (templatingengine.js:67)
	at generateFile (<eval>:77)
	at mcu_CodeGenerator (mcu_codegen.js:36)
	at createTemplatesPerComponent (<eval>:430)
	at main (<eval>:498)
	at <program> (<eval>:547)
	at Clock_Ip_PBcfg_H (clock_utils.js:1790)

 

 

And a screenshot of exactly what I'm seeing in the IDE:

dustinr_0-1736460484773.png

0 件の賞賛
返信
1 返信

1,158件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi Dustin, 

as I said in second thread, RDT is not supported on Linux host and it is not tested. 

0 件の賞賛
返信