S32DS 3.5 Ubuntu 20.04 Install Stuck

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32DS 3.5 Ubuntu 20.04 Install Stuck

13,978 次查看
michaelkehinde
Contributor I

S32 3.5 Design Studio Installer Hangs at "Checking if you already have SW32_S32DS_3.5 license..." at 6%. Followed all steps in the installation guide

InstallerStuck.png

20 回复数

9,568 次查看
jav3251
Contributor II

I have exactly the same problem. Is there really no solution for this?

0 项奖励
回复

9,561 次查看
jiri_kral
NXP Employee
NXP Employee

Hi,

did you tried install latest S32DS v3.6? It uses different Java version and there is high chance that the issue will be solved. 

0 项奖励
回复

9,540 次查看
jav3251
Contributor II

Hi,

Yes, I tried to install the version 3.6.

I tried with java-11 and java-21, with exactly the same result with both - installation is stuck to the screen shown in the opening post.

0 项奖励
回复

9,510 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

S32DS v3.6 requires Java 17. Did you met all requirements for Linux installations? In attachment is Installation guide. 

0 项奖励
回复

9,499 次查看
jav3251
Contributor II

Hi,

I tried with java-17, and then also with 11 and 21. But I did not meet all the other requirements, as I'm running Ubuntu 24.04 - some required packages are not available for it. I installed whatever was available though.

The installation guide says "S32 Design Studio for S32 Platform 3.6.0 supports all editions of the operating systems listed above and is limited only by the requirements of the Java Runtime Environment." which I interpreted as supporting other Ubuntu editions too. But is it so that only  20.04 is supported?

 

标记 (1)
0 项奖励
回复

9,490 次查看
jiri_kral
NXP Employee
NXP Employee

S32DS was tested only with Ubuntu 20.04. It is probably possible run S32DS on newer versions, but it is not tested and you need to use some hack skills. 

I'm mostly Linux guy, but there is less than 5% S32DS downloads for Linux (which is in my opinion sad), that's why there is OS version restrictions and you need to install manually 32 bit libraries and so on. Also some features like RTD is not supported on Linux version. 

 

0 项奖励
回复

11,473 次查看
ranahzzz
Contributor I

I am also facing the same issue. 

Is there another way to install? just unpacking some zip files or something?

 

thanks

0 项奖励
回复

12,330 次查看
adamski
Contributor I

I am also facing same issue. What is the timeline for a resolution? Installation gets stuck at 6% every time. Tried installing with and without a network connection. Is there an offline method for activating the Design Studio 3.5 on Ubuntu 20.04?

0 项奖励
回复

12,764 次查看
LovroJ
Contributor I

Hi,

I'm having the same issue where the S32DS 3.5 installation hangs on Ubuntu 20.04. I found the error log which is attached below. What can I do to fix it?

Best regards,
Lovro

12,758 次查看
jiri_kral
NXP Employee
NXP Employee

Hi Lovro, 

thanks a lot for the Java error log! We aren't able to reproduce the issue, but hope that log file will help to find root cause of the issue. I'll be back when we found solution. 

 

0 项奖励
回复

9,894 次查看
tulips-cirque
Contributor I

Hi,

I'm still facing the same issue. Is there a known solution at this point or at least a known cause?

Thank you

0 项奖励
回复

12,720 次查看
LovroJ
Contributor I

Hi jiri_kral,

thank you for responding and looking into the issue. Here are some additional information so we can rule out potential causes.

1. I checked the integrity of the downloaded installer and it's correct.

 

lovro.jakic@ra-b203-ltu:~/Downloads$ md5sum S32DS.3.5_b220726_linux.x86_64.bin 
65e7ede55835608c44731a1eaaad60a2  S32DS.3.5_b220726_linux.x86_64.bin

 

Screenshot from 2024-02-15 12-19-35.png

2. FNPLicensingService is successfully installed and active. "fnp_install.log" is in the attachments.

lovro.jakic@ra-b203-ltu:/usr/local/share/FNP/service64/11.18.2$ ./FNPLicensingService -r
Licensing Service daemon already active

lovro.jakic@ra-b203-ltu:/usr/local/share/FNP/service64/11.18.2$ ./FNPLicensingService -s
11.18.2.0:x86_64:19862:0

 

3. There are no other errors in logs, except for that java one in the previous response, but regardless, I will attach the ones that I found "e10144dd18dac94b818.details" and "lax-8586466944735677875-err.tmp".

 

4. I checked the shared libraries required by the "libcll_app_libFNP.so" which failed in that Java log and everything looks fine to me.

lovro.jakic@ra-b203-ltu:/tmp/696291.tmp/cll/x64$ file libcll_app_libFNP.so
libcll_app_libFNP.so: ELF 64-bit LSB shared object, x86-64, version 1 (SYSV), dynamically linked, stripped
lovro.jakic@ra-b203-ltu:/tmp/696291.tmp/cll/x64$ ldd libcll_app_libFNP.so
	linux-vdso.so.1 (0x00007ffe243d2000)
	libpthread.so.0 => /lib/x86_64-linux-gnu/libpthread.so.0 (0x00007f604daa3000)
	libm.so.6 => /lib/x86_64-linux-gnu/libm.so.6 (0x00007f604d954000)
	libgcc_s.so.1 => /lib/x86_64-linux-gnu/libgcc_s.so.1 (0x00007f604d939000)
	libc.so.6 => /lib/x86_64-linux-gnu/libc.so.6 (0x00007f604d747000)
	/lib64/ld-linux-x86-64.so.2 (0x00007f604e59a000)
	libdl.so.2 => /lib/x86_64-linux-gnu/libdl.so.2 (0x00007f604d741000)

 

If you have any suggestions or need additional information, please feel free to contact me.

Best regards,
Lovro

0 项奖励
回复

12,948 次查看
swhite39
Contributor II

I am having the same problem. Has there been any progress on debugging the issue?

 

0 项奖励
回复

12,945 次查看
nitish2
Contributor I

Hi swhite39,

No resolution for this stuck issue as of now. Support was also provided by NXP team itself over the call for the installation, but no any breakthroughs. NXP team is checking at their end right now.

0 项奖励
回复

13,087 次查看
nitish2
Contributor I

Hi all,
I am also facing the same installation issue on ubuntu 20.04. Is there resolution for this issue? 

0 项奖励
回复

13,731 次查看
Van1331
Contributor I

Was this solved? I am dealing with this as well and need this to be able to reflash a board that has stopped booting.

13,870 次查看
ashaydesai
Contributor II

Yes, I am also facing same issue. it tries to execute commands from /tmp/ path in my case and stucks at same step.

Also when I restart PC it successfully pops up license prompt,but even when correct key is entered it installation never proceeds any further.

ashaydesai_0-1670433905923.png

 

 

0 项奖励
回复

13,914 次查看
michaelkehinde
Contributor I

Hi Jiri, 

Thank you for your response. Is there anything I can send on my end to help with the process? Please let me know 

0 项奖励
回复

13,932 次查看
jiri_kral
NXP Employee
NXP Employee

Hi Michael, 

 

there is couple similar issues - we are looking at it. It looks, that the installer in some particular cases is stuck with trying to connect to license server, but the reason is not known yet. 

Today I tried reproduce it on my side, but no success. 

 

0 项奖励
回复

13,336 次查看
arynderman
Contributor I

I'm stuck on this as well with S32DS 3.5, Ubuntu 20.04. Is there a resolution?

0 项奖励
回复