S32DS 3.5 Debug issue with O3 optimization

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS 3.5 Debug issue with O3 optimization

ソリューションへジャンプ
3,259件の閲覧回数
Li_Chen
Contributor III

I update my S32DS ID to 3.5 and running the Port_Example_S32K344 example on S32K3X4EVB-Q172 board using PEmicro Debugger. It works as expected, but If I changed optimization level from -Os to -O3, I encountered the 'Break at address "0x0" with no debug information available, or outside of program code' error and cannot debug any more. I'm using SW32K3_RTD_4.4_R21-11_3.0.0_D2303_DS_updatesite

debug_setting.png

 

debug_error.png

 

0 件の賞賛
返信
1 解決策
3,186件の閲覧回数
Li_Chen
Contributor III

I find the root cause is inside startup code. If change Optimization level to Os in the Startup_Code folder, the code could run as expected. 

Startup_Os.png

If Change to O3, the problem will happen after vldr d7, [r1] instruction inside startup.c/init_data_bss function. This is corresponding to the c code ram[j] = rom[j]; where is to copy rom data from __INIT_INTERRUPT_START address 0x00400800 to __RAM_INTERRUPT_START DTCM address 0x20000000. If using Os settup, the assembly is using different instruction ldr.w r7, [r1, r4, lsl #2] and str.w r7, [r0, r4, lsl #2].

Wondering If you have any better explanation or workaround about failure case if using O3 optimization.

O3_1.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,187件の閲覧回数
Li_Chen
Contributor III

I find the root cause is inside startup code. If change Optimization level to Os in the Startup_Code folder, the code could run as expected. 

Startup_Os.png

If Change to O3, the problem will happen after vldr d7, [r1] instruction inside startup.c/init_data_bss function. This is corresponding to the c code ram[j] = rom[j]; where is to copy rom data from __INIT_INTERRUPT_START address 0x00400800 to __RAM_INTERRUPT_START DTCM address 0x20000000. If using Os settup, the assembly is using different instruction ldr.w r7, [r1, r4, lsl #2] and str.w r7, [r0, r4, lsl #2].

Wondering If you have any better explanation or workaround about failure case if using O3 optimization.

O3_1.png

 

0 件の賞賛
返信
3,161件の閲覧回数
Li_Chen
Contributor III
Add volatile to those variables fix the issue:
volatile const uint32 * rom;
volatile const uint8 * rom8;
volatile uint32 * ram;
volatile uint8 * ram8;
0 件の賞賛
返信
3,220件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @Li_Chen 

Check the following post. It has information related to the topic that might be useful to you. 

Is the MCU function and performance exactly the same for (-O3) and (-Os)?

 

B.R.

VaneB

0 件の賞賛
返信