S32DS 3.4 configtools component function list

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32DS 3.4 configtools component function list

2,809 次查看
fk1
Contributor I

Hi,

 

I'm moving form S32 2.2 to 3.4

in the 2.2 version when using processor expert it would show a function list which you could drag and drop into the code, with the configuration names prefilled.

 

does this exist in version 3.4? if so how do i view this

 

Thanks

 

example of what i can see in version 2.2

S32 2.2 processor expertS32 2.2 processor expert

0 项奖励
回复
5 回复数

2,788 次查看
mikedoidge
NXP Employee
NXP Employee

Hello @fk1,

Unfortunately, that functionality was not reproduced in the new S32 Configuration Tools. It was quite a useful feature.

Best Regards,

Mike

0 项奖励
回复

2,567 次查看
yyds
Contributor II

Without this functionality, how does this version call generated functions?  

标记 (1)
0 项奖励
回复

2,554 次查看
mikedoidge
NXP Employee
NXP Employee

You will have to add them using the traditional method. If you are looking for some tool to place the calls into your code, there isn't one.

There are many example projects provided with the SDKs/RTDs which demonstrate the usage of each of the functions.

Best Regards,

Mike

0 项奖励
回复

2,545 次查看
yyds
Contributor II
  • The traditional way? could you make that clear? Thanks

标记 (1)
0 项奖励
回复

2,503 次查看
mikedoidge
NXP Employee
NXP Employee

What I mean by traditional way, is whatever method you normally would use to implement an SDK into your C code without the use of any special tools.

 

0 项奖励
回复