S32DS 3.4 configtools component function list

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS 3.4 configtools component function list

3,663件の閲覧回数
fk1
Contributor I

Hi,

 

I'm moving form S32 2.2 to 3.4

in the 2.2 version when using processor expert it would show a function list which you could drag and drop into the code, with the configuration names prefilled.

 

does this exist in version 3.4? if so how do i view this

 

Thanks

 

example of what i can see in version 2.2

S32 2.2 processor expertS32 2.2 processor expert

0 件の賞賛
返信
5 返答(返信)

3,642件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @fk1,

Unfortunately, that functionality was not reproduced in the new S32 Configuration Tools. It was quite a useful feature.

Best Regards,

Mike

0 件の賞賛
返信

3,421件の閲覧回数
yyds
Contributor II

Without this functionality, how does this version call generated functions?  

タグ(1)
0 件の賞賛
返信

3,408件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

You will have to add them using the traditional method. If you are looking for some tool to place the calls into your code, there isn't one.

There are many example projects provided with the SDKs/RTDs which demonstrate the usage of each of the functions.

Best Regards,

Mike

0 件の賞賛
返信

3,399件の閲覧回数
yyds
Contributor II
  • The traditional way? could you make that clear? Thanks

タグ(1)
0 件の賞賛
返信

3,357件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

What I mean by traditional way, is whatever method you normally would use to implement an SDK into your C code without the use of any special tools.

 

0 件の賞賛
返信